Part Number: TPS2511
Other Parts Discussed in Thread: TPS2041
Hi
Our customer going to use TPS2511. However their condition is the following;
- No negotiation
- only DCP
- charge current max 500mA
- for iPhone and Android
- power supply is by TPS56120
I think that the USB switch (TPS2511) not only used but also the load switch device(with current limit) can be used for this application if the negotiation is not needed.
Could you give me any advice or recommended solution ?
Regards,
Koji Hamamoto