Hello
Do i need to puton some external resistors for unused inputs?
can i allowed SN65LVDS125A inputs open or VCC/GND direct conecting.
thanks a lot.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
Do i need to puton some external resistors for unused inputs?
can i allowed SN65LVDS125A inputs open or VCC/GND direct conecting.
thanks a lot.
Hi Hiro,
If the input is unused, it is okay to use without external resistor. Since the input is not used, we recommend that you disable the unused input by pulling DE for that input high. Disabling the channel will prevent the outputs from toggling due to environmental noise.
Regards,
Michael