Part Number: SN65DP159
Hi team,
The customer is using SN65DP159. He refers to the SLLA358 document. When he writes 0x03 to the register 0x0E
("{0x0E, 0x03} , //CDR_CONFIG[4:0]. FIXED,LN0" on page 9), then the value that he read is 0x01.
Q1: He would like to verify if the read value 0x01 is correct.
Q2: The customer would like to get the complete code of SLLA358 or more code examples. Do we have this?
Q3: If the HPD_SRC pin is pulled down to the low level, then there is not any AUX and DDC signal output.
And his PC will be stuck once the pin is pulled down to the low level. Would you provide some suggestions?
Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments