Hi team,
My customer is intend to kick off an E-mirror project, and the resolution is 1280×720×60fps, the output PCLK is 16bit 70MHz YUV422, or 8bit 140MHz, so I wondering if DS90UB933/934 or DS90UB953/54 could support this application?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer is intend to kick off an E-mirror project, and the resolution is 1280×720×60fps, the output PCLK is 16bit 70MHz YUV422, or 8bit 140MHz, so I wondering if DS90UB933/934 or DS90UB953/54 could support this application?
Fery,
For DVP solution, the present solution in the industry, including our UB933/913, can't support 16bits data per 1 PCLK. So for this case, you can't use the 16bits per 1PCLK.
You can try the UB935/936 solution for low cost high performance.
best regards,
Steven