Part Number: SN65HVD234
Hi,
the max. output current of my DC/DC is only 60mA. I would like to know if this power supply is sufficient.
In the datasheet Icc is specified without load an so not helpful. The max. diferential output voltage is 3V. Hence the max. output current with 60Ohm load is 50mA. This means that the supply current is 50mA plus the current consumption of the chip. Is my consideration right? I use the chip in a network up to five nodes. The other nodes have 5V transceivers. So maybe also common mode currents must be considered.
Can you please specify the max. current consumption with 60Ohm load.
Thanks?
Daniel