Hello,
I want to connect the DP83867IR (RGZ package) to an RJ45 with integrated magnetics. However, the capacitance values of the center tap of the magnetics is only 0.01 uF instead of 0.1 uF, recommened in the data sheet. As well, the capacitance at the cable side (connected to the R 75 ohm to Gnd) has value only 1 nF instead of 10 nF.
Are these capacitance vaulues still in the acceptable range?
Target RJ45 with integrated magnetics:
Recommended Diagram for DP83867IR:
Thank you very much.