Other Parts Discussed in Thread: TPD8S009, TPD4E02B04
Hi
I want to use TDP158 as HDMI redriver.
On the pins i want to use, DP and HDMI share the same set of interface pins.
And according to product design guide, it requires series AC capacitors and pull-down to HDMI compliant (please refer to Figure1)
<Figure1>
So I placed TDP158 next to pull down and series resistor(for HDMI2.0) to make it HDMI compliant. (like Figure2)
But i'm not sure it's OK.
TDP158 datasheet says it is level shifter redriver ac-coupled HDMI signal to TMDS.
If this is the case like Jetson TX2, pull-down and resistor not required.
TDP158 datasheet(Figure3) shows that it uses series capacitor on source side, but i'm not sure i can use pull-down and series resistor.
<Figure2>
<Figure3>
<Question>
1. Should i use pull-down and series resistor on the source side of TDP158 or just capacitor?
2. Can i directly connect the sink side of TDP158 to HDMI connector without any EMI/ESD elements?
Thanks.
Sujin.