Other Parts Discussed in Thread: DS110DF111, DS100DF410
We are using internal PRBS generator for testing. But oscilloscope show could not recovery clock.
We had configed with the sequen below:
p i2c_write_byte(0, 0x70, 1, 1) //I2C switch
p i2c_write_byte(0, 0x18, 0xff, 0x7) //select chanel
p i2c_write_byte(0, 0x18, 0x00, 0x04) //reset retimer
p i2c_write_byte(0, 0x18, 0x2d, 0x89) //set post-emphasis
p i2c_write_byte(0, 0x18, 0x15, 0x52) //set amplitude
p i2c_write_byte(0, 0x18, 0x14, 0x80)
p i2c_write_byte(0, 0x18, 0x09, 0xec)
p i2c_write_byte(0, 0x18, 0x1b, 0x00)
p i2c_write_byte(0, 0x18, 0x08, 0x07)
p i2c_write_byte(0, 0x18, 0x18, 0x00)
p i2c_write_byte(0, 0x18, 0x1f, 0x52)
p i2c_write_byte(0, 0x18, 0x1e, 0x99)
//PRBS_31
p i2c_write_byte(0, 0x18, 0x30, 0x0a)
//PRBS_9
p i2c_write_byte(0, 0x18, 0x30, 0x08)
p i2c_write_byte(0, 0x18, 0x0d, 0x20)
The datasheet has some incorrect discription, so i Refer to the configuration mentioned in the link below
what can i do next?