Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9557: about PCA9557 I/O impedance

Part Number: PCA9557

hi dear supporting team,

for PCA9557 I/O,  besides P0, all other ports has no high impedance mode, correct?  tks!

  • Hey Vera,

    The answer really depends:

    1) If the ports are all set as inputs, then all the pins would be high impedance.

    2) If all the ports are outputs, the pins with a push pull design should always be applying a bias voltage (0V or Vcc) at the gate and turning on a FET (p or n) resulting in a low impedance path on the output. With P0, the design is an open drain. With 0V applied on the gate, the FET will not be turned on and will act as high impedance. However if Vcc is applied to the gate, the FET will turn on as a low impedance path to ground.

    You can see a simplified internal schematic on the datasheet on pages 13 and 14. (Figures 17 and 18)

    Thanks,

    -Bobby

  • hi Bobby,

    ok! thanks a lot!