Part Number: TPS2041C
Other Parts Discussed in Thread: TPS2041, TPS2061, TPS2513
Hi
I would like to ask about the following application note. That is mentioned about the configuration with a power supply and load switch (such as TPS2041 and TPS2061). (please see figure 4)
http://www.tij.co.jp/jp/lit/an/slva049/slva049.pdf
This configuration is very simple.(This configuration (single port) is what the customer want. )
Does this configuration support iPhone and Android?
The customer's condition; no emulation and Io=500mA(max) and D+/D- is connected with <200ohm.
Regards,
Koji Hamamoto