Part Number: TUSB211
Other Parts Discussed in Thread: TUSB212
Hi,
We have a 4-slot CPCI backplane.
We have USB2.0 HS/FS/LS signals interfaced between the daughter cards via the backplane.
Please note that the system has to support live insertion of the daughter cards & the daughter cards should also have the required signal conditioning circuit as well.
As the trace length between the 2 slots is close to 18", we are planning to use TUSB211IRWBR as repeater in both the daughter cards.
The overall end-to-end trace length of the signals can go upto 18" (considering the trace lengths within the daughter cards & the backplane)
Let me know if the TUSB211 part is fine to use for the backplane sort of application for signal conditioning & live insertion for USB2.0 interface.
Looking forward for your suggestion in this regard.