Part Number: TCA9617A
Hi,
Could you help check the SDAA/SCLA pin status with below condition?
- EN is low.
- VCCA (3.3V_stdby) is present
- VCCB (3.3V) is NOT presen
Many thanks!
Bell
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9617A
Hi,
Could you help check the SDAA/SCLA pin status with below condition?
Many thanks!
Bell
Hello Bell,
You have pull up resistors R2061 and R2062 on the SCLA and SDAA, the voltages therefore should be 3.3V assuming R166 and R167 are not populated. If they are and are connected to something else, it will depend on what it's connected to.
Are you seeing something you aren't expecting on those lines? If so, could you please post oscope shots of SDAA and SCLA. Please also look at VCCA and VCCB to ensure they are the voltages you expect (USE OSCOPE).
Thanks,
-Bobby
Hey Bell,
When the EN pin is pulled low, it turns off the drivers which pull the SDAA/SCLA and SDAB/SCLB low or high.
From the figure above, you can think of it from pin 2 to pin 7 and from pin 3 to pin 6 as an open circuit. So you shouldn't see an issue with the SDA/SCL pins being pulled to ground.
Thanks,
-Bobby