Part Number: TUSB422
I am developing a battery charger based reference design using TUSB422. I have the following questions about the diagram:
1. Why the FETs at the input of the charger?
2. Why the boost converter? To provide OTG boost?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB422
I am developing a battery charger based reference design using TUSB422. I have the following questions about the diagram:
1. Why the FETs at the input of the charger?
2. Why the boost converter? To provide OTG boost?
Thanks.
Jeff,
1) DRP can source or sink power so only one path can be enabled at a time.
2) VBAT is typically 3.7V. VBUS is at least 5V (can be up to 20V with USB-PD).
You may want to talk to Steve Schnier who has already developed a charger and sink using this part.