This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75ALS181: ESD ratings

Expert 8760 points

Part Number: SN75ALS181
Other Parts Discussed in Thread: THVD1552

Hi team,

My customer wants to know following ESD ratings of SN75ALS181.

 ① HBM
    ・ Bus terminals
   ・ All pins except Bus terminals

    According to following E2E thread, HBM rating is 2KV.
    Is the Bus terminals HBM rating 2KV too?

    E2E thread: e2e.ti.com/.../631841

 ② Contact discharge, per IEC 61000-4-2 : Bus terminals
      If you have the data, please let me know.

 ③ Air-gap discharge, per IEC 61000-4-2 : Bus terminals
      If you have the data, please let me know.

Best regards,
Fumio Nakano

  • Hello Nakano-san,

    Yes, the bus terminal HBM tolerance would be 2 kV as well. Unfortunately, this device was not designed or tested to meet any level of IEC 61000-4-2, and so we cannot assume much about its performance. If you are looking for a device with IEC 61000-4-2 immunity, I would suggest the newer THVD1552 device. It uses the same pinout as SN75ALS181 but is rated for 30 kV HBM, 18 kV IEC 61000-4-2 contact discharge, and 25 kV IEC 61000-4-2 air discharge.

    Max
  • Hello Max-san,

    Thank you for your prompt reply.
    Your answer is very helpful for us.
    Thank you!!

    Best regards,
    Fumio Nakano