This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90LV004

Expert 1070 points

Hi,

Can you please refer to the following questions for the PN: DS90LV004TVS:

  1. May I assume that the inverting and non-inverting inputs of each channel are interchangeable? Meaning, can I input the ‘P’ signal to the inverting inputs and the ‘N’ signal to the non-inverting input?

           I will have to swap the outputs accordingly, of course.

 

  1. Can I tie the inverting input via pull-up  to VDD rather than GND, and the non-inverting pull-up via pull down to GND rather than VDD?

Thanks