Part Number: TMDS181RGZEVM
Other Parts Discussed in Thread: TMDS181
Hello,
We are testing with EVB and found some issues.
<common setting>
1. Lane / Polarity Swap = Disabled
2. Clock Input Signal Detector = Enabled
3. HPD_AUTO_PWRDWN_DISABLE = Disabled
4. Device Function Mode = Retimer Mode across full range 250Mbps - 6Gbps
<question>
1.On 3840x2160 UHD and 4096x2160 4K resolution
- TMDS_CLOCK_RATIO -> 1/10 of TMDS bit period
- HDMI Clock Rate -> 300MHz
** We can read above status and cannot see any video on the sink with a 4K setop box.
** From the PLL status it togges lock and unlock irregularly.
** It is OK without the EVB.
Can TMDS181 work with 4K resolution? Is there any limitation?
2. Is it possible to tansmit 4K resoution with TMDS Clock Ratio 1/10 of TMDS bit period?
3. What is a right value for transmit termination when the source is 4K and TMDS clock ratio 1/10.
- No termination? or 150 to 300 ohm?
Regards
Kenick