Other Parts Discussed in Thread: DS90UB913A-Q1, DS90UB953-Q1
I see different recommendations for coupling capacitors for the older DS90UB913A-Q1 vs the new DS90UB953-Q1. If I use the larger (100nF / 47 nF) AC coupling caps as suggested for the DS90UB913A-Q1, will that prevent the use of the DS90UB953-Q1 in the same design? I'd like to end up with a design I can use for cameras that use either serializer. I have seen the recommendation for power over coax filter that supports both, so I'm guessing this should be possible.