Part Number: TPS25740
Duplicated the TPS25740EVM-741 design but having issues when plugging a device (cell phone) with a Micro-USB B connector. I have a USB Type-C to Micro USB B cable adapter with the Micro USB B plugged into the phone and the Type-C connector plugged into my design. If I plug the Type-C cable connector in one way it charges the phone, if I flip the Type-C cable connector and plug it in no charging. Not sure what's going on reviewed my design and the TPS25740EVM-741 schematic and they are pretty much the same. Has anyone else seen this and if so what's the solution.