Part Number: TUSB8041A
Hi Team,
My customer is considering using TUSB8041A, but would like to control each of the 4 port individually. Is the TUSB8041A support individual port enable/disable?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi JMMN,
My customer would like to select the port/ports to be enable/disable during the start up (BIOS configuration). In this case, how to configure the register? Is it via USED[3:0] in Port Configuration register (table 5)? Their upstream port is USB3.0.
I only find 6 setting here, but in table 15, it mentioned that each bit corresponds to each port, except ports 1 and 3 disabled. Could advise how to set individual port enable/disable?
You can use the USED register bits to enable / disable the ports. As noted, the only invalid combination is if you try to mark both ports 1 and 3 as disabled at the same time. If all your ports will be USB 3.0 capable and removable (no permanently connected devices) - the USED register is the only one you need to set.
Regards,
JMMN