Hello,
I have a some problems with SATA Gen 3 support
In my system I use Kontron COMe module with 4x ports with SATA Gen 1/2/3 support
Port 0 and Port 1 use SN75LVCP601 redrivers and work well in SATA Gen 1/2 and not work in SATA 3 mode.
Port 2 and Port 3 have direct connection with SSD`s and work well for all speeds with standard SATA cables.
SN75LVCP601`s on ports 0 and 1 drive a backplane with special SSD carrier module connected with backplane.
Distance from SN75LVCP601 to COMe about 4 inches, and from SN75LVCP601 to SSD about 10 inches.
Could anyone recommend re-driver settings for my setup, please?
Default settings (EQ1,2 = 0 dB, DE1,2 = -4 dB, DEW1,2 =1 LONG) work for GEN2 and not work for Gen 3.
-- Regards, Victor