Part Number: TPD1E05U06-Q1
Other Parts Discussed in Thread: TPD2E2U06-Q1, TPD1E05U06
Dear support team;
I downloaded s-parameter model from the following site.
- TPD1E05U06-Q1
- TPD2E2U06-Q1
/cfs-file/__key/communityserver-discussions-components-files/138/4265.TPD2E2U06Q1.s2p
And I shared s-parameter models for TPD1E05U06-Q1 and TPD2E2U06-Q1 with my customer.
But my customer's use case is up to 8.5GHz.
1) TPD2E2U06-Q1 model
This model is up to 4GHz.
If you have the model of up to 8.5GHz, could you share me?
Or could you make it?
2) TPD1E05U06-Q1
This model is up to 10GHz.
But this resolution is 26 points.
If you have the model of more than 1000 points, could you share me?
Or could you make it?
Best Regards,
Masaaki Sugiyama