Part Number: SN65CML100
Hello,
I read through "E2E SN65CML100: Using VBB for single-ended interface"
1. Please confirm that it is enough to simply have a divider using vbb and providing 1.4V at the Pin B, also any recommendations on resistor values? 23.3K and 10k ok?
2. I've tried to simulate this in Hyperlynx but I ended up having to add a 50 Ohm pulldown on Pin A to remove major noise on the top and bottom of the square wave signal. Is this an ibis model issue?
3. does the voltage divider threshold of 1.4V need to change for a 2.5V signal?
thanks,
Adam