Part Number: DS125BR401A
Dear Team,
Could you help to explain the meaning of the register 0x28 bit 0:1 reduced signal detect gain?
Does it means that the amplitude of signal detection signal will become lower for the power saving?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS125BR401A
Dear Team,
Could you help to explain the meaning of the register 0x28 bit 0:1 reduced signal detect gain?
Does it means that the amplitude of signal detection signal will become lower for the power saving?
Thank you.
Hi Jim,
In general we are not recommending to utilize the reduced gain function in the signal detect circuit.
This setting will not save power.
This low gain setting will reduce the sensitivity and bandwidth of the signal detect circuit. These changes can make operation at 6 Gbps and higher very sensitive to the input pattern and amount of attenuation in the channel connected to the DS125BR401A B-side inputs.
Regards,
Lee