Part Number: TUSB1210
Hi Team,
I have customer that would use TSUB1210-Q1 with Jacinto6 6.
The TUSB1210 would be configured as input clock mode then. But the clock coming out from SOC is in tuning yet, not in good ppm quality.
So customer would like to check, if they could use one Active crystal with sine waveform output for PIN26 / 60Mhz ?
I see that REFCLK pin has square wave requirement if being used, but no description on CLOCK pin 26.
Thanks.
4.7.2 ULPI Input Clock Configuration