Part Number: SN65HVD1785
I have been using SN65HVD485 on my slave boards, on my new board I need to change to SN65HVD1785 . The master is an ILX34_MBS485 from Prosoft, running at 19200 .I have 20 slaves on the bus and I am getting some SN65HVD485 failures, always short circuit between V+ and A or B. I have no ringing on supply or comms cables. There may be issues of mis-wiring by operators in the field so I need a device with protection.
Unfortunately the SN65HVD1785 is not working as a direct replacement and I can only get it to work if I pull the output to 5V via a 390 ohm resistor.
I posted this problem previously, but it was nor resolved.
Thanks,
Bertie.