Part Number: ISO5451
Other Parts Discussed in Thread: ISO5851
Hi, I am looking to use the ISO5451 (or similar) to drive a high voltage MOSFET (e.g. IXTF1N400) and I had the following questions:
1. What differences need to be taken care of when using the ISO5451 to drive a MOSFET instead of an IGBT? It is not completely clear from the datasheet.
2. My MOSFET will be connected as a "floating" high side switch (i.e. not ground referenced), is this possible with the ISO5451 please?
thanks
Nick