Other Parts Discussed in Thread: DS90UB913A-CXEVM
Hi Sir
May we know why HS/VS/PCLKO/Lock..... so on need put 10K resistor to GND? can we let these pins pull high?or removed them also be acceptable?
Bogey

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir
May we know why HS/VS/PCLKO/Lock..... so on need put 10K resistor to GND? can we let these pins pull high?or removed them also be acceptable?
Bogey

Bogey,
sorry I can't understand your issue well. please see UB914A d/s for I/O description.
regarding on the pull-up resistor, it is recommended for un-used input pins, which is one general design rule for cmos IC. thanks.
best regards,
Steven
Hi Steven
the customer will use diferential cable(STP), but he reference DS90UB913A-CXEVM and question the 913A(p.21) pin12/pin13 connect to P1 pin1/pin3(pair A1). but 914A(P.25) pin41/pin42 connect to P1 pin4/pin2(pair 2). he wonder is it correct or something wrong here.
May you also help double check circuit as attached?