This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD1S514: TPD1S514-1

Part Number: TPD1S514

A concern for application is protection for USB automotive environment -  especially Cranking and load dump protection.

Can you please inform us regarding:

Is TPD1S514 -1 UL and CB listed?

What is the failure mode of the TPD1S514-1: undefined or open?

TPD1S514-1 EIC 61000-4-5 surge specification:

  • What model do TI use for the 61000-4-5 100V spec: series resistance of 42 Ohm?
  • What is the clamping voltage of Vbus_con: appropriate 35v as in datasheet fig 8?
  • In the TPD1S514 datasheet chapter 8.3.8 a 900W value is stated: is this a 8/20uSec value ?
  • What is Energy rating of the surge protection ?