Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH0318: Read / Write via 8-bit SPI PIC24E Inteface

Part Number: LMH0318

Hi,

I would like to use a LMH0318 with a PIC microcontroller (SPI controlled) but I am facing an issue when I read the datasheet. Currently I can't test the interface and code made to drive the chip.

Anyway, in the datasheet, in the SPI protocol part, it is said that Each SPI transaction to a single device is 17 bits long [...]. But the PIC only support 8-bit or 16-bit format (to send or receive). How am I supposed to do ? The only thing I can think of is to send 3 bytes (so 8-bit format) with :

- First byte contains R/W bit and ADDR[7:1] ;

- Second byte contains ADDR[0] and DATA[7:1]

-Third byte contains DATA[0] and dummy data (7 bits).

Is that so ? Will the LMH0318 discard the last 7 bits (dummy bits) ? Nothing is said in the datasheet (or I missed it).

Thanks for your help !