Part Number: ULN2004A
We use the ULN2004AN (DIP) as a relay driver, in automotive application, so that the working voltages never exceed 14V / 15V, we attach the electrical circuit of the application, which we have been manufacturing for years. You may notice that the incoming signals are from the vehicle's lights.
The problem we have for some time, is that some ULN2004AN burn for no apparent cause, since they work well, and then "stick" some outputs and the tablet has burn, left unused outputs and other times are activated more than one output both. The consumption per output is approximately 30mA per relay.
You would need to know clearly if it is possible to have voltage with a input voltage of 14V on the ULN2004AN, since the input resistance uses the integrated itself.
We used more than 1500 ones. annually of the ULN2004AN, and those that failed are about 30/40 units but ALWAYS after having worked well previously. Will it be within the estimated volume margin of failure?
I appreciate your help with this problem.
Greetings from Argentina.