Part Number: SN65HVD72
Other Parts Discussed in Thread: THVD1520
Hi,
We were recently troubleshooting an RS485 Modbus RTU network which had approx 40 x SN65HVD72 Slave nodes, the problem started when the Master node (SN65HVD72) created a lot of network errors (i.e. could not make sense of the data on the network). We started disconnecting the slave nodes from the network one at a time and eventually found the culprit node which was bringing the whole network down. We replaced the faulty node with another node and everything worked fine thereafter. Unfortunately, we were not able to bring the faulty node back from the plant and it is still with the plant engineer.
Going forward, I was wondering if there is a unit load test that we can perform on the slave nodes at the production stage.
As potentially we can connect up to 200 SN65HVD72 transceivers, the idea is to check the integrity of every single SN65HVD72 transceiver by simulating198 slave nodes and one master node (SN65HVD72), the master node would communicate with the SN65HVD72 slave node under test and if the device communicates without any errors this would be considered a pass.
My questions are:
Is the above-discussed test a fair test?
What sort of setup do we need to simulate 198 additional nodes (SN65HVD72)?
Any help would be much appreciated, thanks in advance.