Is the production 954 EVM suitable for EMC testing a remote camera product? The 954 EVM would be in the chamber with the remote camera.
Is the 953 EVM suitable for EMC testing an ECU with 954 in the design?
If the answer is no, are there alternate platforms to independently test a camera with a 953 and separately an ECU with the 954?
Thank you.