Part Number: SN65HVD230
Vcc and Ground are OK
I see data on the D input; 1's and 0's toggling.
Rs Pin is pulled down.
I see good data on the CAN-L line (data is toggling like the D input) but the CAN-H line is stuck high.
Output is terminated with two, 120 ohm resistors; one on each end.
I tried 2 parts - both with the same issue.
Thank you for any help you can give me.