Part Number: TL16C752D
Other Parts Discussed in Thread: TL16C2550
Hi team,
My customer has following two questions.
(1)Does carrier detect on /CDA and /CDB pins generate a modem status interrupt?
I sat MCR[3] to1 and /CDA to 0, but interrupt did not occure.
(2)If TL16C752D carrier detect on /CDA and /CDB pins does not generate a modem status interrupt,
do you have a device pin-compatible with this device that generates interrupts by these pins?
As to (1), there is no description about /CDA and /CDB pins interrupt on the datasheet.
So, I don't think /CDA and /CDB pins generate a modem status interrupt.
As to (2), TL16C2550 is pin-compatible with TL16C752D. And I think TL16C2550 /CDA and /CDB pins
generates a modem status interrupt. Is this correct?
Please let me know the answers.
Best regards,
Fumio Nakano