Part Number: DS90UB948-Q1
Hi Expert,
My project will choose digital MIC in panel side, can I connector the DMIC to DS90UB948?
Because the datasheet shows the I2S supports Dout. Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB948-Q1
Hi Expert,
My project will choose digital MIC in panel side, can I connector the DMIC to DS90UB948?
Because the datasheet shows the I2S supports Dout. Thanks!
Hi!
Can i join topic?
We are going to use DS90UB948 in conjunction with D-class power amp. TAS5760.
It demands:
MCLK- master clock
SCLK- bit clock
LRCK- Word Select Clock
SDIN- Data Line
So, we suggest, that we have to use pins of Deserializer in a such way:
DS90UB948 | TAS5760
1. MCLK to MCLK
2. I2S_CLK to SCLK
3. SWC to LRCK
4. SDOUT to SDIN
So, i see, that we have pins, that is a master or slave mode.
As i understand- MCLK and SDOUT generates signal all the time, independently of master/slave mode.
But we need to use I2S_WC and I2S_CLK. So we need to activate them through register and use together with the master pins?
Thank you for attention.