Hello,
I have to convert a Display Signal to HDMI and I try to convert it as fast as possible. I need to create a second HDMI connection.
The Board (IMx6) I use has a 24bit RGB interface, another 24bit RGB interface which is converted to 18bitVGA and a dual chanel LVDS interface.
I would like to convert the dual channel LVDS interface to HDMI, but I have seen that there are only ICs that convert HDMI to LVDS and no LVDS to HDMI.
I think the VGA will be very slow, because it is converted from the 24bit RGB.
Which chip ( or chips) should I use to achieve my goal?
What is the fastest way and why?
Thanks a lot