Part Number: TS3USB3000
Dear TI Support,
I'm looking at a design that 's using the TS3USB3000.
On the input to the D+/D- is either LVDS (+/- 1.2V) or SERDES (+/+ 200mV). The OE line is grounded (Active) and the select line is used to select
between LVDS and SERDES. There is an LRC on each of the USB+/- of 10UH, 10ohms and 10UF. I was told that this is needed to
bias the TS3USB switch and to turn it on on power up. Once the capacitor charges up the LRC is not in the circuit anymore.
Does the TS3USB need to be biased? I didn't see this anywhere in the data sheet?
Thanks,
Jeff Cohen
Dentsply Sirona Inc Long Island City NY 11101