Part Number: DP83848C
Hi,
We have a DP83848C PHY which is being destroyed by Power-over-Ethernet transients.
I am adding TVS protection to the PHY side of the magnetics. For now I'm adding 2 back-back 3V diodes as per some recommendations I've found on the web, but I'm not convinced this is the correct solution.
I'm puzzled by the datasheet absolute maximum ratings for this chip, as they claim to be -0.5V to Vcc+0.5V - fair enough for the logic signals, but the magnetics interface is differential about Vcc, so I don't understand the Vcc+0.5 limit and wonder if the ratings for the magnetics interface are different. (e.g. I found an SMSC PHY with a 6V rating).
I'd appreciate any assistance in clarifying what the limits are and whether there are any recommended TVS diode configurations to prevent damage.
Thanks,
Rob