Part Number: TUSB8041-Q1
Other Parts Discussed in Thread: TUSB8041
Hello,
I have a design where I use th TUSB8041-Q1 as a hub and there are USB2.0 and USB3.0 devices connected to the down stream ports of the hub.
I experience connection aborts to the devices connected to the down stream ports. To test this, I connected a USB2.0 USB stick and ran a continous read/write tests and after leaving it for the night I somtimes get a connection failure. And all devices connected to the downstream ports get disconnected at the same time when the error occurs.
I designed the hub with the layout recommendations in mind and tried to stick to the designs suggested in the datasheet.
How can I trace the cause of the error? Could it be a wrong configuration with the Misc I/Os of the hub? I suspected maybe there is an issue with suspend mode with one of the devices.
I have an EEPROM connected to the hub that I don't use right now.
I can provide the full schematic per email.
Thanks in advance.