Part Number: TLK110
Hi Expert,
We meet an problem for Ethernet test for RX+- and TX+- differential amplitude test.
The standard require:
The differential amplitude from receiver side should be 1.9V<RX+-<2.1V, which is the standard PMD amplitude.
However, from customer board which use TLK110, the differential amplitude is around 1.6V.
The schematic is just look like the EVM, and Auto-negotiation with 10/100M half/full duplex mode is used.
Is there any error can lead to low differential amplitude?
Thanks
Zhou