This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVCP408: Questions on output lane-to-lane skew optimization and switching input selection

Part Number: SN65LVCP408


Below are the requirements and information that’s not in the datasheet and I’d to get asap.

  1. Differential clock switching (1MHz to 500MHz)
  2. Any input to any output
  3. Any input to any groups of outputs (including all outputs)
  4. Maintain output-to-output skew per specs (max 75ps) for outputs with same input source
  5. Local Clock Switching: 8 in x 8 out. Best fit found on TI website is SN65LVCP408 (75ps).

Q1: Can I turn off Equalization/Pre-emphasis for better skew?

Q2: Do you have 3*sigma skew number for the chip? It should be less than 75ps.

  1. Output frequencies can change on the fly when switching frequency sets

a-       No glitch is allowed for outputs with no frequency change

Q3: Is each output mux (circled in red below from p.2 of datasheet) completely independent of the others?

b-      Glitch is ok if input changes frequency

c-       Glitch is ok if output selects a new input         

  1. Also need bigger Clock Switch: 18 in x 32 out

Q4: Does TI have any Crosspoint Switch to meet this large switch requirement?

Thanks,

Quang

  • Hi Quang,

    A1:  Turning off EQ and/or Pre-E will not change the skew numbers.

    A2: I do not have the 3-sigma number for output skew.  I just have the typical and max as given in the datasheet.

    A3: Each of the inputs drives an independent 8:1 Mux

    A4: I am unaware of any larger crosspoint switches 

    Regards,

    Lee

  • Hi Lee,

    Thank you for those answers. Can you provide the lowest differential clock speed that can be used? I need 1MHz.

    Support for 500KHz is even better.

    Thanks,

    Quang

    1.       Differential clock switching (1MHz to 500MHz)