Dears
There is a question about DS90UB925. The input signal is RGB888, Can I use UB925 to match the UR906 in the screen ? if can, is there some special note ?
BTW, if the Des UB948 is in the screen , can I use the UB925Q to match it ? pls help to confirm ?