This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP401: Jitter in HSYC output at 1280 x 1024, 60 Hz

Part Number: TFP401


Hello support team,

I have a question about the DVI receiver TFP 401.
Jitter is appeared in the horizontal synchronous output signal of TFP401 48 pin (HSYNC terminal).
There is no jitter in other output signals.
Jitter only occurrs at specific frequency and specific resolution. (1280 x 1024 @ 60 Hz)

Question
As a cause of jitter, is there a possibility that the connection between the board and the thermal pad on the back side of the IC is weak?

Best regards,
M. Tachibana