Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB914A-Q1: Eye diagram

Part Number: DS90UB914A-Q1

Hi,I got the following questions from one of my customers,that would like to measure eye diagram at receive side:

  -should this be done at pins 38-39 (CMLOUP,CMLOUTN) after internal equalization filter, where the back-channel signal is removed?

   -is there a suggested procedure to do this, as we did for PIXEL CLOCK jitter in: “130517DS90UHB925 Jitter Measurement Criteria_5_17_13, DS90UH/B925 Jitter Measurement Criteria (Rev.4), Texas Instruments”

   -CMLOUTP/N are differential outputs; do you suggest to do measurements using oscilloscope differential probes(even if RIN+/RIN- are single ended with RIN- to 50 Ohms)

   - Jitter measurement on this device can be done with a similar procedure as in above document?

Thanks

Umberto