Part Number: DS90UH948-Q1
Hi,
I confirmed function of 0x02[5] (Auto Clock Enable).
Here is procedure which I performed.
1. Connect DS90UH929 EVM and UH948. And power on both EVMs.
2. Set internal pattern generator of DS90UH929. (Confirmed 25Mhz clock at UH948 OLDI pin and "LOCK" is high.)
3. Set 0x02[5] to 0x1 (Enable Auto clock Enable)
4. Disable internal pattern generator (Confirmed "LOCK" is low.)
I believe that I can see frequency which is set to 0x24[2:1] on CLK pin of OLDI.
However, I could not observe any frequency at CLK pin of OLDI.
Is there any incorrect procedure ?
Best Regards,