Part Number: TCA9803
Other Parts Discussed in Thread: TCA9509
I need to use a part which has low VOL levels and VIL levels >0.5 V (on the 3.3V side) for my application where i am level shifting from 3.3V to 1.8V. The TCA9803 seems like a very good fit, however the Vil is mentioned as 0.3*Vcca/Vccb and a note is mentioned saying this is for the first LOW seen. what about subsequent LOW levels? (Typically this is called out as Vilc in other datasheets like TCA9509) Can i assume that a VOL of 0.5V will keep the bus LOW for subsequent cycles as well?
Also, in other level shifter datasheets (like TCA9509) why is it that the Vilc is mentioned only for one side? (in this case, SCLA/SDA)