This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: DP83867

Part Number: DP83867IR

DP83867IR RBIAS issue:

Please claify that voltage at RBIAS should remain constant 1.0V after booting also or will go off to 0V later.

In my board RBIAS voltage I am getting 1.04V when board boots and later goes off to 0V.

Also put some light on functionality of RBIAS resistor.

Regards

Vikrant

  • Hi Vikrant,

    Sleep modes may cause the RBIAS voltage to drop to 0V. What conditions are you seeing the RBIAS voltage drop low?


    The RBIAS resistor has a voltage created by a bandgap circuit. The RBIAS resistor then sets up an accurate current that is used in line driver of the DP83867IR.

    Best Regards,