Part Number: TCA9555
Hi Folks,
I've got a few of these IO expanders in a system where there are some other I2C slaves with 10-bit addresses and would like to run the bus in 10-bit mode. I've briefly tested the expanders and it seems that they do not ACK (ignore the upper address bits) back when my bus is running in 10-bit mode, they do however work perfectly in 7-bit mode.
Question is, should these io expanders work ok if they receive a 10-bit address (i.e. just ignore everything but the 7bits and RW bit).
Thanks,
Peter.