Other Parts Discussed in Thread: TUSB1310
I wonder whether the TUSB1310 provides full support for the optional USB On-The-Go (OTG) protocol detailed in the On-The-Go and Embedded Host Supplement to the USB 2.0 Specification.
If yes, what revision?
The only piece of information I could find in the official TUSB1310 documentation is the following:
" ... The PHY can power down all blocks except the full speed receiver, OTG comparators, and the ULPI pins. ... "
- Fabio