Part Number: TUSB8041
Section 7.6 of the datasheet states that Td1 requires VDD33 stable before VDD is stable. However, footnote 2 states that VDD must be stable >= 10us before VDD3 if using the 1 uF GRSTn capacitor. These two requirements appear to be in conflict.
Also, 9.2.1.2.7 states "The 1 uF capacitor on the GRSTN pin can only be used if the VDD11 supply is stable before the VDD33 supply." This again appears to be in conflict with the first statement in 7.6.
Finally, the reference platform schematic (http://www.ti.com/lit/pdf/sllu198